alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon

Using a Phase Diagram for Vapor Pressure Curves

analytical-instrumentation-phase-diagrams

Using a Phase Diagram for Vapor Pressure Curves

While phase diagrams are primarily used by chemists in laboratory environments, these tools can be astonishingly useful for mechanical engineers and plant managers tasked with sample analysis. In some analytical systems, a liquid sample must be converted to gas through vaporization before it can be analyzed. Vaporization is essentially a balancing act between temperature, pressure and flow variables – and a phase diagram’s vapor pressure curves allow engineers to identify phase changes for distinct materials and chemical compounds.

Contact YOUR SWAGELOK SALES AND SERVICE CENTER

As you read on, a hypothetical gas mixture of 20% hexane in pentane will be applied as a complete phase diagram (see diagram below). When the sample is above the bubble point (blue line), it will be entirely in the liquid phase. A sample must remain in its liquid state as it enters the vaporizer. When a sample is below the dew point (gold line), it’s all vapor. The sample must be all vapor when it leaves the vaporizer.

Using a phase diagram for vapor pressure curves

Between the bubble point and dew point lines is the “no-go zone.” This zone represents the boiling range of the sample. Here, the mixture is in two phases: part liquid and part vapor. Once a sample falls into the no-go zone, it is fractionated and no longer suitable for analysis. The objective of vaporization is to set the temperature, flow and pressure so that the sample skips instantly from the liquid side of the no-go zone to the vapor side. With pure and nearly pure samples, there is little to no boiling range or no-go zone. The bubble point and dew point lines are simply on top of each other or nearly so.

Pure and nearly pure samples will convert to vapor of the same composition, whether through evaporation or vaporization. Some industrial samples approach this level of purity and convert fairly easily. On the other hand, some samples have such a wide boiling range or no-go zone that they cannot be successfully vaporized. There is no way for such samples to skip from the liquid side of the no-go zone to the vapor side. In this case, variables cannot be manipulated to avoid fractionation.

In the diagram shown above, the band between bubble point and dew point is narrow enough that with the proper settings, the sample can effectively skip from the liquid side of the no-go zone to the vapor side. At the same time, the band in the diagram is wide enough that one cannot afford to be careless.

Setting Temperature, Pressure and Flow

Continuing to work with the sample in the diagram (20 percent hexane in pentane), inputs need to be skillfully set to ensure successful vaporization. In general, high pressure and low temperature is needed at the inlet. Conversely, at the outlet, high temperature and low pressure is necessary. There are limits as to how high and low these parameters can be, and not every constraint can be controlled.

1. Determine the Inlet Pressure at Your Vaporizer

The inlet pressure, which is fixed, is the process pressure—provided that the vaporizer is located near to the sample tap. In the example diagram, that pressure is 4 bar. Higher pressure is better because it allows the vaporizer to keep the temperature higher without boiling the incoming liquid.

2. Set the Inlet Temperature

When setting the inlet temperate, there are two objectives. First, the temperature must be low enough that when the sample enters the vaporizer, it is entirely a liquid. In the example diagram, the bubble point at 4 bar is 88°C. To guard from fractionation, it is best to choose a round number far enough away from 88°C to avoid the no-go zone. A safe example temperature could be 80°C.

The second objective is to keep the temperature high enough to contribute to the complete flashing of the sample—ensuring only vapor leaves the vaporizer. When vaporizing a sample, the temperature drops in accordance with the laws of energy conservation. The sample temperature must be high enough at the outset so that after the pressure drop the sample does not fall in the no-go zone. In the example diagram, the vapor temperature after the pressure drop is 60°C—just on the vapor side of the dew point line.

3. Set the Outlet Pressure

When setting the outlet pressure, the objective is to drop the pressure below the dew point line. In the example diagram, the outlet pressure is set to 1.5 bar. If the outlet pressure were any higher, the sample would not vaporize entirely and would fractionate.

4. Set the Flow

Flow is set downstream at a valve and rotameter, not at the vaporizer. In a sampling system, high vapor flow is desirable because it moves the sample to the analyzer faster. However, high flow can be problematic because more heat is required to vaporize the sample. In other words, high flow results in a greater drop in temperature at the time of vaporization. In the example diagram, the purple line illustrates the temperature drop. As the flow increases, the temperature drops sharply.

Another variable influencing the temperature drop is the heat transfer capability of the vaporizer. Some vaporizers are constructed in such a way that heat transfers more efficiently to the sample. When the liquid sample converts to a vapor and its temperature drops, it draws heat from the stainless steel surrounding it. The critical question is how efficiently the vaporizer can replace the heat and keep it flowing to the sample. The more heat the sample can draw, the less its temperature drops during vaporization. In some instances, it is possible for the vaporizer to be hot to the touch on the outside but cold at the core inside. That’s because the vaporized sample is drawing a high amount of heat and the vaporizer cannot transfer enough energy to keep up. The best solution is to reduce the flow.

In sum, the temperate drop visualized in the diagram is a product of the flow rate and the heat transfer capability of the vaporizer. With a good quality vaporizer and low flow rate, the line in the diagram will become more vertical. Unfortunately, there is no easy way to calculate the precise location of the temperature drop within a phase diagram, and it cannot be generated by any known software program. As a result, vaporization involves some approximation. As a rule of thumb, keep the flow rate as low as possible without causing an unacceptable delay in the sample’s travel time to the analyzer. It’s better to start with a low flow rate and experiment by increasing it than to start with an initially higher flow rate.

For additional help with analytical instrumentation and sampling system best practices using phase diagram vapor pressure curves, please contact your local Swagelok sales and service center.

Contact YOUR SWAGELOK SALES AND SERVICE CENTER

Related Articles

position-nozzle

How to Position Nozzles in Your Liquid & Natural Gas Sampling System

The details can make all the difference in sampling system efficiency. Avoid analysis delays, sample contamination, & inaccurate results in your liquid or gas sampling system by adhering to these nozzle placement best practices from Swagelok analytical instrumentation expert Karim Mahraz.

process-analyzer-sampling-system

5 Common Process Analyzer System Revelations over 50 Years of Training

Sampling systems can be one of the most challenging systems within your plant to both design and operate. Industry veteran and industrial training instructor, Tony Waters, shares his trainees’ top revelations over the past 50 years.

ten-tips-sampling-systems

10 Tips to Improve Sampling Systems

Managing an analytical instrumentation operation is no small feat. Receiving consistent results can be a struggle for even the most seasoned engineers. Luckily, there are several simple tips your team can use to improve your sampling system.